AnsweredAssumed Answered

Differntial OPAMP with input CM voltage 0.5 to 0.75

Question asked by elc.manas@gmail.com on Mar 15, 2016
Latest reply on Apr 21, 2016 by daverowe

Dear All,

 

We need a Differntial OPAMP which can tolerate input common-mode voltage variation from 0.5 to 0.75 V , the output differntial swing peak-peak voltage can go up to 2.4 V (each side give an aplitudue of 1.2 V).

Also the OPAMP should have low input referred noise and high linearity.

We want to use it as an RC low-pass filter.

 

Could anybody please tell what can be the best OPAMP available with AD ?

 

Kind Regards,

Outcomes