AnsweredAssumed Answered

AD9361 :  how connect CNTRL_IN, CNTRL_OUT,  DIG_IO

Question asked by marcob on Mar 14, 2016
Latest reply on Mar 22, 2016 by mhennerich

Hi,

 

I must design a system with 4 chip AD9361 and I'm using FMCOMM5 as REFERENCE DESIGN.

 

The discrete In/Out (CNTRL_I , CNTRL_0, and others ) are connected to the GPIO(63..0) of CPU ( GPIO via EMIO).

When I use  four chip AD9361  where  can I interface the digital In and Out signal ?


The LIB IIO is configured to accept   4 channel ?

Can I use AXI_GPIO to connect digital IO between  FPGA and AD9361 ?


Thanks in advance

Marco


 

Outcomes