AnsweredAssumed Answered

FEEADR0H is *two bits* wide

Question asked by tcachat on Mar 14, 2016
Latest reply on Mar 21, 2016 by ABuda

Dear all, in the datasheet UG-367 (rev. D) for the ADuCM360_361, page 93 of 176, I read:

     "FEEADR0H is two bits wide",

but on the table below only one bit, bit 0, has a significant value... I suppose it should be bits 0 and 1, to allow access to the information space at address 0x20000? Same question for FEEADR1H.

 

Sorry if this is trivial. There is no 32-bit register FEEADR0 directly available?

Outcomes