AnsweredAssumed Answered

Adding 2 AD9361 Cores into Vivado Design

Question asked by USDseniors on Mar 11, 2016
Latest reply on Mar 17, 2016 by USDseniors

I am using 2 FMCOMMS3 SDRs and the ZC702 evaluation board.  I am creating the block diagram of my system using the libraries provided by Analog Device.  After building all the libraries into Vivado, this is the project block diagram.

.block_diagram.PNG

  This only includes one AD9361 core in the design.  Since I have two SDRs, I know that I need two AD9361 cores.  Below is a picture of the AD9361 block on the right and the input ports on the left.

core_ports.PNG


What do I need to do to support both SDRs?  Is it as simple as creating another AD9361 block, and input ports?


Thanks for any help in advance!

 

Outcomes