AnsweredAssumed Answered

Input voltage abs max

Question asked by mhz on Mar 10, 2016
Latest reply on Jun 22, 2016 by mattholland

The absolute max ratings in the BF70x datasheet state -0.33V to 3.60V. Does this mean that BF70x inputs can be driven by 3.3V logic, even when its VDD_EXT is running from 1.8V with no issues of latchup or forward biasing protection diodes?

Outcomes