AnsweredAssumed Answered

HMC627ALP5E amplifiying issue

Question asked by ahmet783 on Mar 11, 2016
Latest reply on Mar 18, 2016 by kkaya

Hello everyone

I have a custom rf board with three cascaded connected hmc627alp5e in IF side of RF card. IF signal frequency is 70 MHz and when 70 MHz -50 dBm if signal is applied to input of the three cascaded hmc627alp5e, I get -53 dBm signal output side. Based on the datasheet value, I expect around 0 dBm signal. spectrum analyzer display picture is attaced. input and output rf line is designed 50 ohm and component value is selected based on the "50-350 MHz" configuration in the datasheet page 9. I can control attenuator side of component via SPI but amplifying is not enough value that is given in datasheet.  Anybody know how to solve this issue

 

Thanks in advance

 

Ahmet

Attachments

Outcomes