AnsweredAssumed Answered

ADXL343 vs ADXL345

Question asked by bvn123 on Mar 10, 2016
Latest reply on Mar 12, 2016 by neilzhao

Hi

what kind of differences are between ADXL343 and ADXL345,

except samplerates below 6.25Hz for ADXL343?

 

In Selection Table (the link is here: Selection Table for MEMS  Accelerometers )

Bandwidth -3dB for ADXL345 is 1.6kHz and only 0.32kHz for ADXL343

 

But it seems 0.32kHz for ADXL343 to be mistake,

cause in the Datatsheet the highest samplerate for ADXL343 is 3200Hz and appropriate bandwidth 1600Hz

Outcomes