AnsweredAssumed Answered

AD9910 Higher Frequency output

Question asked by FreddyS on Mar 9, 2016
Latest reply on Mar 9, 2016 by JLKeip

Dear supporter

We  are curently using the AD9910 in our design (@ Fout<400Mhz).

We would like now to use the same AD9910  to generate a signal up to 500MHz.

Question:

1) Is the AD9910 able to support it? I know it is limited to 400Mhz by spec but in fact we can work with it up to 430Mhz

 

 

2) Is there any possible "sqeeze" to get higher Fout? of course with degradation of some other parameters.

 

3) If we use a higher sampling rate (1.1GSPS for example):

     - What will be affected from this higher sampling rate?

 

 

 

Thanks

Freddy

 

 

 

 

Outcomes