AnsweredAssumed Answered

EVAL ADAS1000SDZ - Mounting Holes on the PCB

Question asked by kurt63 on Mar 8, 2016
Latest reply on Mar 8, 2016 by CatherineR

Hi!

 

I have bought the Evaluation board "ADAS1000SDZ" and other necessary isolation-Boards. I want to build an Multichannel ECG-System for education purposes – not for clinical applications.

 

All those boards should be functionally integrated in a modern instrument-case.

Unfortunately - the ADAS1000-pcb has no predrilled mounting holes.

But - it seems, that there are predefined drilling spots at the four edges of the pcb.

 

After removing the 4 rubber distance-holder at the bottom side of the print:

 

Is it possible to drill a mounting hole with  3.2mm  diameter at each of those spots, without negativ effect to the functionallity of the ECG-board?

Are there any risks with the multilayer-board - even if we made precision-drills?

 

The save mounting of the "eval-board ADAS1000" is mechanically very complex without those holes!

I would appreciate your informations to this question and looking forward to your replies!

 

Best regards!

Kurt

Outcomes