AnsweredAssumed Answered

multichannel input/output evaluation board

Question asked by ryan_s on Mar 6, 2016
Latest reply on Mar 9, 2016 by DaveThib

I'm working on a project at school and the first step is to choose a dsp/evaluation board but I'm having trouble. The project is to create a system that can be used for a variety of audio applications (such as sound localization or digital effects processing). Because of this the evaluation board should have at least 3 inputs and 1 output. Some other requirements at 16 bits/sample and at least a 16KHz sampling rate and the ability to operate in real time. The final result should be a setup where to do a new audio project, one would only have to do simple coding (preferably C, or maybe python). Thanks for any help, feel free to ask more questions about the project.

 

Ryan

Outcomes