AnsweredAssumed Answered

HMC-T2220B outdoor application

Question asked by SerP on Mar 4, 2016
Latest reply on Mar 9, 2016 by SerP

Dear sirs,

 

Our customer would like to use HMC-T2220B for outdoor applications. The environment conditions are: -15...+35 degrees (C), hummidity up to 90%.

Operating temperature shown in DataSheet is: 0 to 35 °C. How does the customer can implement this generator if it is possible? Will it be enough to use a termocase?

The customer is also would like to have the Ingress Protection Rating of generator. I can't find this data. The customer needs at least IP54. I've seen this generator and seems like it is not a dust protected device. Do ADI has some kind of protection case for using this product in real outdoor applications?

 

Best Regards,

Sergey Pavlov

Outcomes