AnsweredAssumed Answered

Any way to generate example waveforms other than 2 tone with FMCDAQ2?

Question asked by etroy on Mar 3, 2016
Latest reply on Mar 29, 2016 by DragosB

I am working with the FMCDAQ2 board and the ZC706. Previously, I worked with the FMCOMMS3. In both cases, there are example files for creating complex waveforms like chirps, msk-20M.txt, etc. I was able to get them to generate waveforms with the FMCOMMS3 and ZC706, but, even though I can "load" them into the DAC buffer settings with the FMCDAQ2, nothing happens. Is there a way, using the iio supplied software (or maybe GNU companion, to generate wideband modulated signals with the FMCDAQ2 board when mated to the ZC706?

Thanks in advance.

Outcomes