AnsweredAssumed Answered

AD9467FMC + ZEDBOARD :Modify max buffer dimension on  AXI_DMAC IP

Question asked by marcob on Feb 29, 2016
Latest reply on Mar 2, 2016 by charlyelkhoury

Hi,

 

I'm using  a AD9467FMC-250EBZ + ZEDBOARD, with SDK project.

I use the reference design : hdl/projects/ad9467_fmc/zed at master · analogdevicesinc/hdl · GitHub

I'm using an 80MHz clock ADC.

I must read a buffer of adc sample with a dimension of  64 MByte ( 32 M sample), but the

max dimension of "lenght X" is 16MByte ( only 24 bit is used) in axi_DMAC IP.

 

How can i expand the dimension of data captured without loss sample ?

 

I opened the design firmware and  i saw the possibility of programming the Lenght X and Lenght Y,

Can i use this mode for  my acquisition ? In this case which is the software interface ?

 

Best regards

Marco

Outcomes