AnsweredAssumed Answered

ADV212 IO power supply

Question asked by zhangsan3012 on Feb 28, 2016
Latest reply on Feb 29, 2016 by DaveD

I got the information in adv212 datasheet "2.5 V or 3.3 V input/output and 1.5 V core supply", Now I have to connect ADV212 IO pins to both 2.5V and 3.3V pins of xilinx's FPGA, is that OK or I have to add a buffer to match the interconnect pin's power level? thanks very much.best regards.

Outcomes