AnsweredAssumed Answered

Default configuration AD9212-40 without SPI

Question asked by LeonE on Feb 27, 2016
Latest reply on Mar 7, 2016 by LeonE

Good day.

 

I use AD9212-40 and don't want to configure it by myself, because the default settings suits me. Thus the FPGA, which control pins CSB, SCLK and SDIO connect them to VCC (CSB pin) or GND (SCLK and SDIO pins). I understand correctly, that in this case, the ADC should load with default values and begin to process the input signal and transmit the signal to FPGA?

Outcomes