AnsweredAssumed Answered

ADuC7060/61: A/D performance vs Clock source

Question asked by V.M. on Jun 30, 2011
Latest reply on Jul 1, 2011 by MikeL

In the electrical specs, it is stated that the conditions are:

...Fcore = 10.24 MHz driven from an external 32.768 kHz watch crystal or on-chip oscillator...

 

Is A/D accuracy or noise is affected by its ultimate clock source (e.g. external high-accuracy Crystal or internal 3% Oscillator)?

Outcomes