AnsweredAssumed Answered

Set sampling frequency with Sigma Studio for ADAU1372

Question asked by Clement on Feb 24, 2016
Latest reply on Feb 24, 2016 by DaveThib

Hi all,

 

I'm using EVAL-ADAU1372Z with Sigma Studio and I'm wordering what is the difference between the system sampling rate and the serial port sampling rate ?

Capture.PNG

 

It seems that changing the system sampling rate has no effect on the Fs mesured on the Serial audio port and it's quite weird to set the sampling rate of the device in the serial port parameters.

 

Also, there isn't 44,1kHz as the Serial port FS, is that means that the device cannot work at 44.1kHz ?

 

Thanks.

 

Best regards

Outcomes