AnsweredAssumed Answered

ADL5350 frequency range

Question asked by nithesha.a on Feb 23, 2016
Latest reply on Feb 24, 2016 by nithesha.a

Hi ,

 

I am planning to use ADL5350 for the below applications. Please let me know if the part is suited for these applications:

 

1) RF input 107MHz - 137MHz and IF is fixed at 21.4MHz

2) RF input 107MHz - 137MHz and the IF is varied from DC to 30MHz with LO fixed

 

I would want the mixer to have a reasonably high IIP3 and high input power handling capability. ADL5350 looks impressive!

 

As suggested, i am planning to use ADF4351 for LO generation.

 

Is ADL5350 suitable for these applications? Any issues to be taken care of?

 

Thanks and regards

Nithesh

Outcomes