AnsweredAssumed Answered

Analog Phase Shifter control voltage? HMC-C010 and HMC247

Question asked by MohammedS on Feb 22, 2016
Latest reply on Mar 1, 2016 by SMcBride

Hello,

 

I'm a little confused about the description in the datesheet. It says the the phase is "controlled via an analog control voltage ". However, the provided data sheet gives the performance at with DC control voltages only. The control pins seems to be designed to a DC voltage as well.


Would this "50MHz modulation bandwidth" allow to control the phase by a 10MHz sinusoid for example?

Are there any S11 v.s. Vctl  measurements available?


Thank you.

Outcomes