AnsweredAssumed Answered

ADuC842 now reports itself as an ADuC843 with WSD

Question asked by jeffreyk59 on Feb 20, 2016
Latest reply on Feb 22, 2016 by MMA

I have a design with ADuC842 that has worked for many years.  Recently after using this ADuC842 several times, it now reports a WSD error 6 when attempting to download new code.  I also notice that the MCU now reports itself as an ADuC843 device.  What happened? Is there some DATA bytes that I inadvertently erased that might cause this problem?

 

Here is the resulting string that is captured in HyperTerminal window when the MCU is reset with PSEN held LOW:

ADI 843   V212

 

This used to say:

ADI 842   V217

Outcomes