AnsweredAssumed Answered

For isolated buck converter circuit using ADP2441

Question asked by Laliberte on Feb 19, 2016
Latest reply on Feb 25, 2016 by Jason_Duan

Hi, All.


Using the dual transformer as shown in the figure below we would like to make a circuit in the ADP2441.


<Specifications>
Vin: 24V (32V max)
Vout1: 5V (100mA)
Vout2: 3.3V (100mA)

 

Do you have any problems with the circuit configuration of the above?


Best Regards,

Laliberte

Outcomes