AnsweredAssumed Answered

query about amplitude modualation capability of AD9914

Question asked by Nupur on Feb 18, 2016
Latest reply on Feb 18, 2016 by JLKeip

hii
myself nupur bhangalei have a question regarding amplitude modulation capability of AD9914 
like in my application 63.87MHz carrier sinusoidal signal (generated using DDS) have to be amplitude modulated using discrte value of amplitude  forming sync shape(around 100 points in 3ms time interval)....is it possible using AD9914 evaluation board ? if yes how to do it like what else other device and which pins do i need to configure to implement the design.................

Outcomes