AnsweredAssumed Answered

FMCMOTCON2 custom axi_mc_controller

Question asked by 3ronaldt on Feb 16, 2016
Latest reply on Mar 24, 2016 by ACozma

Hi,

 

I would like to implement a dedicated closed control loop inside the FPGA fabric, using the current measurement as feedback signal.

 

The idea is to change axi_mc_controller block.

 

In the reference design, the adc_data_cx outputs of axi_mc_controller are connected to a DMA controller.

Inside axi_mc_controller the adc_data_cx outputs are directly connected to the ctrl_datax_i inputs (assign adc_data_c0  = ctrl_data0_i).

 

However, the ctrl_datax_i inputs are (intentionally) left open in the Vivado block diagram.

 

Is this correct and is it up to the user to connect the required signals to ctrl_datax_i inputs (for example the axi_mc_current_monitor outputs)?

 

Thanks and regards, Ronald

 

Outcomes