AnsweredAssumed Answered

[ADICUP360]encounter an error message "unable to find CMSIS-DAP device".

Question asked by sofy Employee on Feb 16, 2016
Latest reply on Apr 19, 2016 by jchong
Branched to a new discussion

Hello,

Congratulations releasing ADICUP360.

I have been trying to use ADICUP360 with following wiki information but encounter an error.

(I try to test blink project and GDB OPEN OCD debugger as following on Wiki instruction)


Eclipse fail to download elf file with error message as below.


Open On-Chip Debugger 0.10.0-dev-00025-g81cc011-dirty (2015-08-17-13:23)

Licensed under GNU GPL v2

For bug reports, read

  http://openocd.org/doc/doxygen/bugs.html

Info : only one transport option; autoselect 'swd'

adapter speed: 5000 kHz

adapter_nsrst_delay: 100

cortex_m reset_config vectreset

Error: unable to find CMSIS-DAP device

 

This error seems Eclipse cannot recognize ADICUP360 via USB port. (Because when I unconnected ADICUP360 with PC, Eclipse show the same error message as above.)

I suppose I miss something setting on ADICUP360 board.. But I can not figure out where is wrong...

Jumper and DIP SW setting are default.

 

I've tried also another ADICUP360 and other USB port and cable and several S1-S4 switch combinations but all fail.

I would appreciate if you have any suggestions.

 

Best regards,

Sofy

Outcomes