AnsweredAssumed Answered

BF592 on SPI1 does not boot...

Question asked by hifihi on Feb 10, 2016
Latest reply on Feb 11, 2016 by hifihi

Hello out there,

 

I made a small board with a BF592 that, for some reasons, uses the boot device on SPI1.

Bootmode is set correctly "010" - the secondary loader starts (see attached screenshot), the SPI clock is about 188kHz.

After some 30 Bytes the communication with the M25P16 stopps.BF592_BootStart.jpg

The .ldr file Shows an end address on the last line of 0x3C58, so that can't be all. I have no idea how to get out of this Problem: is it related to the "Anormalies issue", or can I make any test to come closer to a solution: with the HPUSB-ICE it worked perfect.

 

Any help is highly appreciated.

 

Regards

 

Hans Hief

Outcomes