AnsweredAssumed Answered

ADF4360-8 driving AD9268 problem

Question asked by Michitechy on Feb 10, 2016
Latest reply on Feb 19, 2016 by Brigid.Duggan

We use an ADF4360-8 at 125MHz with a successive AD9513 to source 2 AD9268 125MHz/16bit ADCs and a FPGA.

The Lext is 180nH, the reference frequency 24MHz, PDF=1MHz, loop filter 3rd order passive, 105kHz and 44.4deg phase margin.

Almost the recommended values of ADIsimPLL.

The ADC input is driven by an ADA4938-2 differential amplifier. Measuring a grounded input signal we sometimes get the expected good noise data with some 9.5 LSBs FWHM distribution. But then, we as often get additional 282kHz (and harmonics) that distroy the good ADC data.

GND_Noise_good.png

Fig 1: GND noise and its FFT when good

 

GND_Noise_bad.png

Fig 2: GND noise and its FFT when bad

 

We found that this seems to come from the PLL circuitry as a finger on the 2 inductors can fairly influence and improve this behaviour.

Any ideas where this really comes from and how to avoid this?

The inductors are at a 90° angle as recommended.

Outcomes