AnsweredAssumed Answered

AD621 drift with temperature

Question asked by RBC on Jun 27, 2011
Latest reply on Jul 14, 2011 by RBC

I'm using an AD621 in amp to read a pressure transducer. The transducer is excited with -10Volts, the 621 is powered with +/-15Volts. The gain of the 621 is set to 100 ( pin 1 and pin 8 connected). The output of the 621 is being fed to an opamp to provide gain, and then feeds a microcontroller to digitize the voltage. I'm using a linear regulator for the -10V and zener diodes for the +/- 15V.

 

The problem I'm having is a zero drift with temperature. I have built a resistor bridge with the same resistance of the transcuder for testing. While I heat the AD621 and associated circuitry I don't heat the bridge, the bridge remains at abmient temperature. From ambient to 125C the output of the 621 drifts from -.113 to              -.095. The -10V is stable, it changes around 20mV through the heat range, the +/-15V changes more but that change should not be reflected in the output voltage (I don't think).

 

Any ideas on what might be causing the drift? Any comments are appreciated.

Outcomes