AnsweredAssumed Answered

Simple toggle DPI pins

Question asked by ChristianH on Feb 2, 2016
Latest reply on Feb 3, 2016 by ChristianH

Hi,

 

I'm using some ADSP-21489 DSPs and try to find a simple way to toggle DPI pins without using the SRU macro.

The functionality is set once after booting as GPO pin but the status should be changed during runtime.

 

I have used all FLAGS (mapped them to AMI data and address pins and FLAG pins) so I can't do it by set/clr flags ....

I still have signals to toggle but the SRU macro needs 15 cycles each time which I want to avoid (need to save cycles).

 

Is there a way to toggle a DPI (or DAI) pin like e.g. bit set DPI_xxx_whatever BIT_x .... ??

 

Thanks in advance!

Christian

Outcomes