AnsweredAssumed Answered

Warning while building a project for BF561

Question asked by Yaniv.Sapir on Jun 23, 2011
Latest reply on Jun 28, 2011 by Yaniv.Sapir

I used the project wizard to generate a template project of type "Dual core: Single application" for the BF561. The Idle_CoreB project includes a local_shared_symbols.h header while it is not associated with the generated .ldf file. Thus, upon building, it uses the default adsp-BF561.ldf file.

 

However, at the link phase of the build, I receive the following warning:

 

 

 

Linking...
[Warning pp0084] "C:\Program Files\Analog Devices\VisualDSP 5.0 10x\Blackfin/ldf/adsp-BF561.ldf":1038 Include file not found in path; opening in connected directory.
This legacy behavior will not be supported in future releases.
Filename: 'local_shared_symbols.h'

 

 

 

How can I eliminate this warning?

Outcomes