AnsweredAssumed Answered

AD5933 used to measure very large impedances

Question asked by verysmallcap on Jan 28, 2016
Latest reply on Feb 8, 2016 by musach

Hello AD5933 users.
Has anyone used a AD5933 supplemented with a suitable external transimpedance input stage (TIA) to measure very large impedances?

As an example the TIA could be a AD823 with a 10Mohm feedback resistor, set to get the noise budget right.  Our requirement is to measure capacitances in the 10s -100s fF range, amounting to an impedance magnitude of 10s -100s Mohms (at 100kHz).

Outcomes