AnsweredAssumed Answered

Re: AD9361 TX Attenuation

Question asked by bensonyeung2 on Jan 25, 2016
Latest reply on Jan 26, 2016 by tlili
Branched from an earlier discussion

Hi,

 

We have developed our own PCB which is similar to ADI eval board. However when setting Tx attn. in dB using GUI software, we get more power if large value of  attn(e.g. 25dB). is set. We get less power if attn. is set to 0.

 

I)Could there be any calibration issue? When we are using ADI eval board we don't see this issue. We did check the Hardware control line and made sure the schematic/layout is correct.

 

ii) is there another way to set the total Tx path gain instead of just using the Tx attn. in GUI?

 

Benson

Outcomes