AnsweredAssumed Answered

ADIsimCLK with AD9520-5 for Clock Distribution only?

Question asked by schiepep on Jan 26, 2016
Latest reply on Jan 27, 2016 by schiepep

Hi,

 

I want to simulate a loop filter for the AD9520-5 using an external VCO in ADIsimCLK.

For the AD9520-5 there is only a configuration option for clock distribution with disabled PLL (no loop filter, no external VCO).

Can I instead select another AD9520-x and make a simulation with disabled internal VCO? Does all AD9520-x share the same loop dynamics?

 

Furthermore I am unsure if I have chosen the right PLL-Eval-Board for my project in generell.

Goal is to phase-lock an 80 MHz 'slave'-VCO to a 240 MHz reference-source. With the lowest Jitter as possible. Time to lock is not important.

Input signals to the PFD are 3.3V LVPECL.

 

Beside the AD9520-5 I took a look at the HMC984LP4E.

 

It would be great, if you have any advice for me.

Outcomes