AnsweredAssumed Answered

ADF4351:stopping the write sequence

Question asked by ysuzuki on Jan 25, 2016
Latest reply on Jan 26, 2016 by rbrennan

Hello,

 

I have a question about ADF4351.

If the write sequence is stopped before receive 32 clock and then the LE is moved to high, is the broken data thrown away from shift register ?

Or the write sequence is aborted ?

 

If the broken data are not thrown away, and If the LSB 3bits of the broken data are "000", I think the internal registers may be updated by the broken data.

Can ADF4351 prevent this improper operation ?

 

Best regards,

ysuzuki

Outcomes