AnsweredAssumed Answered

Using lower sampling clock for high speed ADC ?

Question asked by Jiwon.Lee on Jan 20, 2016
Latest reply on Jan 21, 2016 by DougI

Dear,

 

As an example,

When using AD9653(Quad, 16-Bit, 125 MSPS, Serial LVDS 1.8 V ADC),

data sheet shows the sampling clock range for this part is 20MHz ~ 100MHz.

If I want to use it with below 10MHz, around 5MHz ~ 10MHz(5Msps ~ 10Msps).

Is it possible ?

If possible, should I add or change some additional circuit ?

Outcomes