AnsweredAssumed Answered

(ADuM321x)WA grade, Maximum data rate

Question asked by donadona999s on Jan 20, 2016
Latest reply on Jan 20, 2016 by donadona999s

Hi !

 

I have two questions about ADUM321x MAX data rate.

 

1)

The A grade's Max data rate is 1Mbps.

Does this spec has margin?

If it has , can you tell me the margin value?  For only advisory is OK, need not to be spec.

I mean ...for example... what will happen if Input Frequency is 1.001Mbps?

I think device will work with normal operation.

 

2)

Also I think the device won't be destroyed if the input frequency is higher than 1Mbps at A grade.

Is my understanding is correct?

 

Best regards.

Kawa

Outcomes