AnsweredAssumed Answered

ADuC7061:Drive capability of I2C-Pins

Question asked by Woodstock on Jan 20, 2016
Latest reply on Jan 20, 2016 by MikeL

Hi,

 

i am using the I2C interface of an ADuC7061. I am using 820R pullups so i draw about 3 mA when SDA or SCL goes down. From the datasheet i know a single pin can sink 4 mA but is there a problem if the I2C pins together draw 6 mA if both Pins are logic 0?

Outcomes