AnsweredAssumed Answered

Single-ended-signal to differential-signal conversion for InAmp test

Question asked by lyto on Jan 19, 2016
Latest reply on Jan 25, 2016 by lyto

Hello alltogheter,

 

I am new at analog circuit design, so I need some help. I bought some Instrumentation Amplifiers: AD8421, AD8428 and AD8429 and the Evaluation board EVAL-INAMP-82Rz for them.

 

I want to test which InAmp is suitable for my application. In order to measure them, i need to provide a differential signal on the input of my Evaluation Board. My differential Signal should have 8MHz bandwidth.

 

I have a ROHDE & Schwarz HF-Synthesizer HM8134-3 that can create a single ended signal from 1 Hz to 1.2 GHz  with -127 dBm to +13 dBm. (I also have a HUBERT A1020-75-250 High Frequency Amplifier, i dont know if i need that) Now I want to convert the single-ended-signal into a differential signal.

 

Is it possible to do that with some of the following Amplifiers:

AD8138 or AD8042 or ADA4941-1 or AD8475 ??

 

It should look something like this. Is this OK?

FrageAD_zone_singleToDiff.jpg

Thank you,

Best regard,

lyto

Outcomes