AnsweredAssumed Answered

VisualDSP++ corruption

Question asked by stevet1976 on Jun 22, 2011
Latest reply on Jun 22, 2011 by CraigG

When I start Visual DSP++ I get an error

 

"Failed to create memory window because the following memory type does not exist in the target hardware Data(DM) memory"

 

Visual DSP++ will start after this error but I can not connect to a session I get the following error

 

"An invalid argument was encountered"

 

I get the same error when I try to exit VisualDSP++.

 

To kill the application, I have to go to windows task manager and kill the application, which still generates the invalid argument error but does also kill the application.

 

I am using VisualDSP++ v5.0 with update 9, running on Windows XP.

 

My target is Sharc21469. The problem started when I powered off my target hardware(custom board) before closing the connection. I have done this many times before and got the standard JTAG can't talk to the hardware errors, but Visual DSP++ has not been corrupted before and has restarted OK.

 

Are there any files that can easily be repaired that would cause this error or do I need to go for a re-install.

 

Thanks

 

Steve Tostevin

Outcomes