AnsweredAssumed Answered

Partial Reconfiguration with FMCOMMS2

Question asked by crimechb on Jan 11, 2016
Latest reply on Jan 11, 2016 by CsomI

Dear Sir,

 

I have checked the wiki.

https://wiki.analog.com/resources/fpga/docs/hdl/partial?s[]=fmcomms2&s[]=pr

 

In Test the design using a Linux image

I have some questions about step 2.

2.Make sure that the BOOT partition of the SD card, contains the correct BOOT.bin, device tree and uImage. (To create the BOOT.bin the user should use config_default.bit bit file)


a. Just modify the config_default.bin to BOOT.bin and copy it to SD card ? (folder \hdl-hdl_2014_r2\projects\fmcomms2_pr\zc706\prcfg_default\bit\config_default.bin)


b. Can I used the same device tree and uImage? (image in zynq-zc706-adv7511-ad9361-fmcomms2-3 folder)



Best Regards,

Paul

Outcomes