AnsweredAssumed Answered

ADV7511 Project with own image processing IP-Core

Question asked by Welee on Jan 11, 2016
Latest reply on Jan 22, 2016 by larsc

 

Hello,

 

I’m really new to hardware design. I have to implement an image processing system on a Xilinx zc702 due to a given task from my university.

 

I got the ADV7511 reference project runing and it's working well.

 

Now I intended to manipulate the image in the vdma with my own IP-Core doSobelHLS (a Sobel-Filter).

 

I've connected the M_AXIS_MM2S from vdma to my Input Stream of doSobelHLS and the output of doSobelHLS to the m_axis_mm2s of the axi_hdmi_tx.

 

After validating the design successfully and an init section in the SDK, unfortunately there’s nothing more than a black screen.

 

I have tried another IP-Core from Xilinx. But there are only white strips appearing on the screen.

 

Besides, I’ve also tried to connect the clock of doSobelHLS to the axi_clkgen and the FCLK_CLK0 of the PS.

 

Totally desperate now – I don’t know any more what else I can do or at what point I’m doing mistakes.

 

Can anyone please help me?

 

 

 

Please find the "hardware design and the init section" attached.

 

Outcomes