AnsweredAssumed Answered

Frequency range of ADL5350

Question asked by jhshin on Jan 11, 2016
Latest reply on Jan 11, 2016 by mthahira

RF, IF and LO frequency range was not clearly described in ADL5350 datasheet.
But, based on applications information in ADL5350 datasheet, I guess that RF, IF and LO frequency range of ADL5350 are LF ~ 4GHz.

Is it right?

 

I want to use ADL5350 as the following frequency.
  RF : 2300 ~ 2400 MHz
  IF  : 640 ~ 740 MHz
  LO : 1660 MHz

 

Could I use ADL5350 in upconverter/downconverter for the above frequency?

 

Thanks in advance.

Outcomes