AnsweredAssumed Answered

ADAU1446 SPDIF recovered Clock as Master

Question asked by Brettcoupe on Jan 10, 2016
Latest reply on Feb 29, 2016 by Brettcoupe

Hi

Is it possible you use the recovered clock from the SPDIF receiver to be the clock source for the SDATA and DSP Core

 

My Project uses external Codec IC  as a slave that is connected to SDATA , and just one SPDIF I/O interface

So If I can Clock the Codec IC and The DSP from the Recovered SPDIF clock then I wont need SRC.

 

Is this Possible , I cannot see where to set the Clock domains to the SPDIF recovered clock.

Thanks

Brett

Outcomes