AnsweredAssumed Answered

ADV7511 RGB Input Format

Question asked by mike.baker Employee on Jan 6, 2016
Latest reply on Jan 7, 2016 by mike.baker

Section 4.3 in the hardware manual states that the input data can be right, center or evenly justified. But Table 16 only provides an example of 12-bit data (Input ID 0). I want to confirm it's possible to right justify RGB data so that R(7:0), G(7:0) and B(7:0) map to D(23:0). My confusion is that the alignment bit, 0x48[5] specifies it's for DDR alignment and 0x48[4] is the bit justification for YCbCr data. If it's possible to right justify 24-bits of RGB data what needs to be programmed?

Outcomes