AnsweredAssumed Answered

ADI Reference Design for ZC702, AD9467_FMC and AD9739a

Question asked by T-D-R-N on Jan 6, 2016
Latest reply on Jul 25, 2016 by ACozma
Branched to a new discussion

Hallo,

I have the same Boards (ZC702, AD9467 FMC and AD9739a) like in this Thread (AD9739A-FMC-EBZ / AD9467-FMC). Based on Istvan advice to include the no-OS Software, I am trying to built the HDL File, first. Afterward I want to export it to sdk and use the no-OS Software, too.

 

For this purpose I have to built my own HDL File because neither the AD9467 FMC nor the AD9739a supports the carrier for the ZC702. My Idea is to built a HDL file with the ADI Reference Designs for one of the supported Carriers (like ZED) and do some changes to get them running on the ZC702. Is this possible?

AD9467_FMC.PNG

Building the libraries worked fine, I also inserted the two missing library cores. But when I tried to build the project for the ZED, I stuck with these Errors, which can be find in attachment.


Can someone help me, please? And is there a better way to get the Board running?

 

Thanks,

Tudo

Attachments

Outcomes