AnsweredAssumed Answered

PL2303 Driver issue with provided Kernel

Question asked by Quamstar on Jan 5, 2016
Latest reply on Jan 5, 2016 by timh

Hey Folks,

 

iam using the zedboard with the newest release of analog devices (Linaro 14.04. Kernel: 3.17.0-g18efa1b) while i was trying to mount a GPS-Mouse to the USB-Port i recognized that there are some issues with the PL2303 usb serial driver.

 

1) When enter "lsusb" in the promt:

Bus 001 Device 002: ID 067b:2303 Prolific Technology, Inc. PL2303 Serial Port

Bus 001 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub

 

2) dmesg | grep USB

ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver

Found TI TUSB1210 ULPI transceiver.

zynq-ehci zynq-ehci.0: Xilinx Zynq USB EHCI Host Controller

zynq-ehci zynq-ehci.0: new USB bus registered, assigned bus number 1

zynq-ehci zynq-ehci.0: USB 2.0 started, EHCI 1.00

hub 1-0:1.0: USB hub found

usbserial: USB Serial support registered for generic

usbserial: USB Serial support registered for FTDI USB Serial Device

usbhid: USB HID core driver

usb 1-1: new full-speed USB device number 2 using zynq-ehci

 

So the PL2303 device will not be attached to any tty.

 

3)  modprobe usbserial vendor=0x067b product=0x2303

modprobe: ERROR: ../libkmod/libkmod.c:556 kmod_search_moddep() could not open moddep file '/lib/modules/3.17.0-g18efa1b/modules.dep.bin'

 

there is no module for the 3.17.0 kernel..

 

4) ls /boot

System.map-3.13.0-24-generic  grub

abi-3.13.0-24-generic         initrd.img-3.13.0-24-generic

config-3.13.0-24-generic      vmlinuz-3.13.0-24-generic

filesystem.dir

 

It shows the 3.13. kernel but not the 3.17.0.. why is the kerne version 3.17.0 (uname -r), and i cannot found anything about it in the system?

 

I hope you can help me

 

kindly regards

Jan

Outcomes