AnsweredAssumed Answered

SSM2166: stereo link, defeat noise gate

Question asked by jon71 on Jun 18, 2011
Latest reply on Jul 22, 2011 by jon71

Questions regarding SSM2166:

 

- when linking two devices for stereo operation, is it possible to link the following pins, using resistors 1/2 the values indicated in the datasheet:  ratio set, noise gate set, rotation set, gain adjust?

 

- can the downward expansion be successfully defeated by feeding a noise signal (or perhaps an ultrasonic tone) mixed into the buffer at a level just above the noise gate threshold, resulting in 1:1 operation below the noise signal level (of course, with the noise-free audio fed directly into the VCA rather than linked from the buffer out)?

 

Regards,

 

Jon

Outcomes