AnsweredAssumed Answered

HMC6981LS6 power off

Question asked by VTesi on Dec 31, 2015
Latest reply on Feb 17, 2016 by VTesi

Hello, we have to develop a switched radar application using HMC6981LS6 PA.

In order to obtain an attenuation of RF power output, is it enough to bring VGG1 & VGG2 to -3 Volt (cutoff?) ? Is this safe? Does the PA maintain stable behavior when VGG is switched from the cutoff value to the value for correct operation ( bias = 1000 mA) ? What are typical values of VGG1, VGG2 for 1000 mA bias ?  Do you have S parameters of HMC6981LS6 when biased at 0 mA ?

 

Does the HMC6981LS6 have any limit in allowed load VSWR ?

 

Thanks, bye

Outcomes