AnsweredAssumed Answered

HMC-MDB277

Question asked by black3 on Dec 29, 2015
Latest reply on Jan 15, 2016 by black3

I have something to ask you about HMC-MDB277.

 

I’m looking for an up-converter which modulates a 73-GHz LO signal with a high-speed(>10 Gbps) baseband data and also a down-converter which operates in the opposite way.
The target application is not related to E-band wireless backhaul. There is another different channel I’ve made for communication in the ~70GHz frequency band.

 

If the several requirements are satisfied, our lab is planning to purchase the product.

 

  1. Is the gMBR0011 suitable to up-convert and down-convert the NRZ/PAM4 data using a LO frequency of 73GHz?
  2. Can you show me data regarding to the return loss at the IF port and RF port?
    I don’t know what kind of bandwidth do the ‘IF bandwidth’ and ‘RF bandwidth’ mean.

  

I’m looking forward to your reply.

 

Have a good time at the end of the year.

 

 

 

Thank you.

 

Outcomes