AnsweredAssumed Answered

I2S audio on AD9889b

Question asked by imran on Jun 18, 2011
Latest reply on Nov 16, 2011 by pratyush

Hi ,

I am facing some issues in playing i2s audio on ad9889b.

My board contains an audio codec STA529 and and HDMI transmitter AD9889b.

same i2s input goes to both sta529 and ad9889b .

When i type the following command:

aplay -f S16_LE -r 48000 -c 2 -t raw -D plughw:0,0 /opt/48_16_2.pcm,

I observe that I am getting audio aoutput from STA529 but not from HDMI receiver.

I am using an HDMI analyzer(Astro-VA-1809A) as HDMI sink and it shows AUDIO FIFO ERROR and PLL lock error in audio timing.

I have tried both manual and automatic methods for CTS.

I am using N as 6144 and CTS calculated in automatic mode is 148230(while playing audio it keeps toggling between 14229 and 14230).

For manual mode I use a value of 74250 as per the programming guide.

In automatic mode I only get audio fifo error but in manual mode i get both audio fifo and pll lock error.

I observe that Audio info frame is correct in both the cases but channel status bit shows audio fifo error and pll lock error.

Could any body please tell me where I am making mistake ?

The value of the audio setup related registers are as follows:

 

0x01----> 0x00

0x02----> 0x18

0x03----> 0x00

 

0x04 =  0x02

0x05 =  0x43

0x06 =  0x06

0x07---->0x01

0x08 ---->0x22

0x09--->0x0a

 

0x0a[7] ---> 1

0x0e = 0x01

0x0f = 0x13

0x 11 = 0x37

0x12 = 0x00

0x13 = 0x00

0x 14 = 0x02

0x15 = 0x20

0x40 = 0x00

0x44 = 0x78

0x51 = 0x00

 

Please let me know where I am making mistake. Is there anything else that I need to check.

 

Thanks in advance,

Imran

Outcomes