AnsweredAssumed Answered

AD9361 and Zedboard bring up issue

Question asked by hajimowlana on Dec 22, 2015
Latest reply on Dec 25, 2015 by hajimowlana

Hi,

 

I have a AD9361 evaluation board and a Digillent Zedboard and I am trying to run the example test provided by Analog Devices. FMCOMMS2. I found the right image online and loaded it into the SD flash card. When I set the jumpers and switches in the right positions as explained in the document and turn on the board, I only see two Linux logo (penguins) on the top left side of the monitor connected to the board through HDMI and nothing else. The monitor is blank everywhere else. Anyone has experienced the same issue? Is it possible that I am using the wrong image? ( I don't think so but it is still possible).

 

Thanks

Ed

Outcomes